Cancel
Showing results for 
Search instead for 
Did you mean: 

X and Y toolbar

Valued Contributor
Valued Contributor

XYtoolbar.png

This toolbar apears in the drafting enviroment on one of our engineer's computers. We have entered values into the fields and nothing on the screen seems to change. Can someone tell me what this bar does and how to turn it off?

 

1 REPLY 1

Re: X and Y toolbar

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Cabinet_Guy  On the Sketching tab in the Grid control section, it's the "XY" button for X Y Key-In is ON.  Toggle it off.

 

It allows an X Y cordinate to be keyed in when drawing elements.  So when it has values in it, when you click to place the start or end point of a line, it is placed at the X Y coordinate listed in that dialog 



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com