Cancel
Showing results for 
Search instead for 
Did you mean: 

XPRESROUTE Flanges Adding

Creator
Creator

XPRESROUTE, Adding flanges
Hello everybody,
Is there anyone who knows a method to finish a line of piping with a flange and a blind flange on the same end.

1 REPLY 1

Betreff: XPRESROUTE Flanges Adding

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Liveclau

 

 

 

I suppose this more is a matter of Piping rather than xPresRoute.

 

With Piping module You also have those standard componets available which are needed for piping and the the pipe between IMHO is done automatically.

 

 

regards
Wolfgang