Cancel
Showing results for 
Search instead for 
Did you mean: 

Xpress Route - Non Independent Model

Creator
Creator

Is there a setting somewhere that I can change so that XpressRoute creates the hose/tube routes only in the Assembly as a reference part and doesn't have to be saved as its own independent component? For example I have an assembly that I want to show plumbing in but I do not need/nor want to have an independent solid file for every routing.

1 REPLY

Betreff: Xpress Route - Non Independent Model

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @C_Berg

 

 

it isn't xPresRoute but if YOu use Frame Design You have it in assembly only!

 



regards
Wolfgang