Cancel
Showing results for 
Search instead for 
Did you mean: 

Xpress route Tube end treatment issue

Pioneer
Pioneer
hi, i am using Solid edge ST4 Xpress route for tube routing. While routing the tube, In end treatment option it is showing (None,Close and Reduce) option. It is not showing Expand type end treatment. Tube dia is .188. anybody can help me on this?
5 REPLIES 5

Betreff: Xpress route Tube end treatment issue

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @balajil

 

 

can You provide a picture what exactly You are looking for?

 

regards
Wolfgang

Betreff: Xpress route Tube end treatment issue

Pioneer
Pioneer
Please find the attached image..

Betreff: Xpress route Tube end treatment issue

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @balajil

 

 

 

suppose You are looking for the end lengthening of end 1 and end 2

 

This is not a treatment but a extension

 

Simply enter the wanted value at End 1 or End 2 position

 

Se20170330_0846.PNGe picture:

 

 

regards
Wolfgang
Highlighted

Betreff: Xpress route Tube end treatment issue

Pioneer
Pioneer
Actually that issue happened due to template. I have changed the template. now it is working fine.

Betreff: Xpress route Tube end treatment issue

Siemens Phenom Siemens Phenom
Siemens Phenom

I am guessing the tube where you were seeing the issue was defined as a solid tube. Expand and Flange treatment types are only available for hollow tubes. This setting is on the Tube Options dialog:

 

tubeoptions.png

 

Hope this helps,

Greg