Cancel
Showing results for 
Search instead for 
Did you mean: 

Zero Thickness Error

Experimenter
Experimenter

I've noticed that some other people have had the same error, but I'm trying to make a symmetric extrusion and it's not allowing me to.Untitled.png

2 REPLIES 2

Re: Zero Thickness Error

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Before extruding hit the "add body" command. Or make the base extend slightly into the feature below it so there is not just a line intersection.

 

AddBody.png

 

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Betreff: Zero Thickness Error

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @inyikos

 

 

 

as already mentioned by @bshand take care that there are no tangent connection between a hole and a outside face, that there are no areas where volume will become zero  - what then simply is called a non-manifold situation.

 

This in reality would also let break any piece of material at the same position into two parts!

 

regards
Wolfgang