Cancel
Showing results for 
Search instead for 
Did you mean: 

activate ST8

Experimenter
Experimenter

I got a activation code for ST8 and when I put this code in the Solid Edge License Utility under "I have an Academic Code" the button for ok does't light up so I can't finish it.

4 REPLIES 4

Re: activate ST8

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there,

 

You will also need to enter the name of the school?

 

ST8_LicenseUtility_AcademicCode.png

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP6] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: activate ST8

Experimenter
Experimenter

Still doesn't work...like you can see I did fill in my school + the key and the button for OK doesn't light up?

Re: activate ST8

Siemens Phenom Siemens Phenom
Siemens Phenom

Have you tried the "Activation Code" option instead of the "Academic Code" option?

Re: activate ST8

Community Manager Community Manager
Community Manager

@Heikki Please send me the academic code you are using via private message, and I will help you debug the problem.

 

Regards,

Laura