Cancel
Showing results for 
Search instead for 
Did you mean: 

add more bends to rounded piece of sheet metal

Valued Contributor
Valued Contributor

I have a sheet metal part that I converted from a surface I create that forms a semicircle (top view).  Its 1/8" aluminum.  To form it we will need a lot more bend lines so that we can form that half circle on the brake as a segented half circle. 

 

How can I do this?  I have attached the file

21 REPLIES 21

Re: add more bends to rounded piece of sheet metal

Honored Contributor
Honored Contributor

If you are trying to "Bump" a sheet into a circle rather than roll it, you will have to model each bend to get bend lines for that.

 

Have fun adding many 175 degree bumps (I hate that they are not 5 degree bumps)

Re: add more bends to rounded piece of sheet metal

Valued Contributor
Valued Contributor

Understood.  Not following that last sentence though

Re: add more bends to rounded piece of sheet metal

Honored Contributor
Honored Contributor

The angle referance use for flanges is the wrong way in my opinion. A very small bend should be 5 degrees not 175 degrees when adding a flange.

Betreff: add more bends to rounded piece of sheet metal

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

HI @lifofadrafter

 

 

and whats about using a Lofted Flange?

 

See example part and picture

 

20170920_1949.PNG

regards
Wolfgang

Betreff: add more bends to rounded piece of sheet metal

Valued Contributor
Valued Contributor

you must be on ST10?  I cant open the file?  That is what im looking for though.  That effect.  how did you do that?

Betreff: add more bends to rounded piece of sheet metal

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @lifofadrafter

 

 

Yes I am using ST10 but this function is there from v10 or even before.

Can't remember when it was introduced.

 

See video to do it Yourself - isn't really that problem:

 

(view in My Videos)

regards
Wolfgang

Betreff: add more bends to rounded piece of sheet metal

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@lifofadrafter,

 

As @hawcad shows, using lofted flange is easiest way to achieve this, the key "option" to use here is the "Triangulation" bending method, which allows the model to look smooth......alternatively, I have used a trimmed polygon sketch to get a real world faceted [using a lower bend count] contour flange [& lofted flange] in sheet metal parts.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Betreff: add more bends to rounded piece of sheet metal

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @SeanCresswell

 

 

 

trimmed polygon sounds great too.

 

Since the polygon function is there why not?

 

regards
Wolfgang

Re: add more bends to rounded piece of sheet metal

Phenom
Phenom
180 is flat, 135 is opened from 90, 45 is tighter than 90, 5 is almost closed.

175 is 5 tighter than 180