Cancel
Showing results for 
Search instead for 
Did you mean: 

Betreff: add more bends to rounded piece of sheet metal

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@lifofadrafter,

 

I'm not sure if it has ever worked in a bend table......but maybe that is why I've always made drafts of sheet metal parts with the triangulated bending method, using coordinate dimensions & a typical bend info callout text.

 

LoftedFlange_TriangulatedBendingMethod.png

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Betreff: add more bends to rounded piece of sheet metal

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @SeanCresswell

Hi @lifofadrafter

 

 

just tested it here with ST10 and Yes, the bend table doesn't show the bend angle of any single triangulated bend.

Only the complete 180 degrees of the complete loft.

 

But using a property text connected to any of those bend lines will bring the right info

 

20171025_0809.PNG

regards
Wolfgang