Cancel
Showing results for 
Search instead for 
Did you mean: 

adding dimension column to the hole table

Creator
Creator

hello Smiley Happy

 

Is there a way to put the dimensions of the holes and the callouts (like a thread) in the same column of a hole table?

In the image, the spaces for the threads callouts are completed right, and the blank spaces were meant to be completed with the diameters, but it doesn´t appear in the table. 

 

Imagem sem título.png

 

I´ll apreciate any help or opinion! Thanks!

 

Bruna

4 REPLIES

Re: adding dimension column to the hole table

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Yes, Make sure for "Callout 1", which I assume is what you are using for your last column, has the Simple hole definition defined as shown below.

2016-06-03_9-36-13.png



Ken
Production: ST10 MP7, Testing: SE 2019
http://Grundey.blogspot.com

Re: adding dimension column to the hole table

Creator
Creator

Hi Ken! 

 

I did that, look:

 

Imagem sem título2.pngBut the table is still empty... Well, I guess I´ll have to make another column just for the diameters...

 

Thanks for your help Smiley Happy

 

Re: adding dimension column to the hole table

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

You shouldn't have to do that.  Are what you think are simple holes really a Hole feature in your model?

A circular cutout is not a Hole and thus has no hole information.



Ken
Production: ST10 MP7, Testing: SE 2019
http://Grundey.blogspot.com

Re: adding dimension column to the hole table

Creator
Creator

Hi Ken,

 

You were right, I thought the holes were hole features, but it wasn´t! I changed the cutouts and it worked!

 

Thanks for your help Smiley Happy