Cancel
Showing results for 
Search instead for 
Did you mean: 

anyone else recently having issues with KeyShot shutting down?

Legend
Legend

I've tried dealing with KeyShot support, but thus far it hasn't improved my situation. For some odd reason, starting early last, KeyShot will shut down when I try to add materials or environment to my project.

 

I've uninstalled, removed all residual folders, installed again, tried Solid Edge install repair, and even tried wearing an aluminum foil hat. I can get it to work after fiddling with stuff, and the next day it won't run.

 

If I have the settings on the main page to use all CPU cores (not rendering screen), my system shows 100% CPU usage when I have a project opened.

ST8 MP9
Go FAST, or go home.
2 REPLIES

Re: anyone else recently having issues with KeyShot shutting down?

Phenom
Phenom

I have 8 CORES on my Dual Xeon CPU system, but I only use 6 for Keyshot. I found it keeps the system from getting too hot, and it really doesn't hurt performance much.

 

Bob

Re: anyone else recently having issues with KeyShot shutting down?

I had it in the past. I just shut down every application when I go render a model.
I also have 8 cores and use them all.
-------
Daniël Schuiling
Solid Edge ST7
Teamcenter 10