Cancel
Showing results for 
Search instead for 
Did you mean: 

anyone still using a Spaceball 5000?

Legend
Legend

Just wondering if anyone is still using the SB5000 or if you gave up on the legacy device and moved to the pro or enterprise version.  I have become too dependant on the button functions but the legacy driver and SE addin are behaving erratic at times. If anyone is using the old SB5000 do you have a config that is working well?  using the 3D Connexion control panel or using the SE addin?  They seem to clobber each other from time to time.  Had mine working well for ~6 months using the 3DC control panel and last Monday the settings were changed and I couldn't figure out what happened.


If you cannot find a Solid Edge setting, confirm you have a file open of the type that will be affected.
11 REPLIES

Re: anyone still using a Spaceball 5000?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Time to give it up I think Smiley LOL



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: anyone still using a Spaceball 5000?

Legend
Legend

I was affraid of that.  Any one switch from the old SB to the new space mouse enterprise or pro?  It looks like the enterprise version goes for ~$260, is it worth the ~$60 more than the pro? Is it worth the $160 more than the navigator?


If you cannot find a Solid Edge setting, confirm you have a file open of the type that will be affected.

Re: anyone still using a Spaceball 5000?

Siemens Phenom Siemens Phenom
Siemens Phenom

Yes, I had to throw it away the other year when the drivers stopped working and there were no new compatible drivers posted. A pity for a still fully working piece of hardware.

 

So I went for the SpaceMouse wireless and getting rid of the cable is a relief. 

 

/Ulf

Siemens EMEA GTAC Support

Re: anyone still using a Spaceball 5000?

Honored Contributor
Honored Contributor

Spaceballs? Their goes the planet!

 

Sorry,  off topic, could not resist

Re: anyone still using a Spaceball 5000?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Spaceballs? Good movie!

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: anyone still using a Spaceball 5000?

Phenom
Phenom

At the office I use a SpacePilot Pro. Good device, but I don't use the screen.

I would suggest the SpaceMouse Pro now. I don't care about the cable, my desk is fixed so once you manage your workspace the cable doesn't bother me anymore.

...........................................................................................................
Solid Edge 2019 & AutoCAD 2019 user

Re: anyone still using a Spaceball 5000?

Siemens Phenom Siemens Phenom
Siemens Phenom

I must admit that the main annoyance with the cable is when travelling.

The old SpaceMouse broke at the cable inlet and the same happened to a colleague.

Siemens EMEA GTAC Support

Re: anyone still using a Spaceball 5000?

Legend
Legend

Thanks all.  Sounds like I need to just get updated.  I don't travel enough to take the 3D mouse with, I'll see if I can get an enterprise, 31 programmable buttons! Smiley Happy


If you cannot find a Solid Edge setting, confirm you have a file open of the type that will be affected.

Re: anyone still using a Spaceball 5000?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@bnemec, Now you are just showing off! Smiley LOL



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com