Cancel
Showing results for 
Search instead for 
Did you mean: 

assembly relationship

Creator
Creator

I am new to solidedge and I am using solidworks..

now I want to learn solidedge

I started that, and now i have some questions.

Please help me to learn it faster.

 

1)Is it any way to know all parts in asssmebly are fully definded?

2)how can I give relationship using part reference plane? 

5 REPLIES 5

Re: assembly relationship

Regarding your first question, yes there is a quick way to determine if a part is fully postioned. See the online help section titled "PathFinder in assemblies," which explains what the different pathfinder icons mean.

 

part_not_fully_positioned.jpgpart_not_fully_positoned_2.jpg

David McMahon
Solid Edge 2019
HP Z2 Mini, Windows 10

Betreff: assembly relationship

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

HI @Raumik

 

 

 

first answer already is given, and the answer to the second question would be "Yes" this also is possible ver easyily.

 

When inserting parts or subassemblies You have to press the "Paste - Construction Display" button.

Here You can temporaraly acitvate the visibility of planes, coordinate systems, surfaces, and so on

 

This is available for the pasting part as wel as for the relation parts.

 

But, this only is true if You turn off the flash fit option in placement

20170813_2130.PNG

regards
Wolfgang

Betreff: assembly relationship

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Raumik

 

 

 

another option would be to turn ON the visibility of planes and coordinate systems during inserting of parts.

 

20170813_2137.PNG

regards
Wolfgang

Re: assembly relationship

Creator
Creator
THANKS FOR THE HELP

Re: assembly relationship

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Raumik

 

welcome, happy to help You

 

regards
Wolfgang