Cancel
Showing results for 
Search instead for 
Did you mean: 

assembly sketch tools greyed out as FamilyOfAssemblies

Legend
Legend

Is there a setting somewhere that needs changed or is dissabling of sketches and features in a FOA expected behavior?

 

I was working on an old assemnbly that has a half dozen sketches and decided to try using FOA during the development stages for different concepts.  Then I try to edit a sketch or create a new one and the menus relating to sketching are all greyed out.  Couldn't figure it out, made a new asm and all sketch menus are fine.  Thought to self, maybe?  changed new asm to family of assemnblies and poof, all sketch related icons on the ribbon turn grey. 

 

Are sketches not supported in FOA files?


If you cannot find a Solid Edge setting, confirm you have a file open of the type that will be affected.
2 REPLIES 2
Highlighted

Re: assembly sketch tools greyed out as FamilyOfAssemblies

Siemens Phenom Siemens Phenom
Siemens Phenom

You have to toggle on/off "Apply edits to all members".

 

With "Apply edits to all members" off then Sketch is disabled:

2018-01-10 16_16_28-PathFinder.png

 

With "Apply edits to all members" on then Sketch is enabled:

2018-01-10 16_17_09-PathFinder.png

Re: assembly sketch tools greyed out as FamilyOfAssemblies

Legend
Legend
Thank you! I had kept that off as I only wanted to edit the active member. I will be toggling that on and off a bunch I suppose.

If you cannot find a Solid Edge setting, confirm you have a file open of the type that will be affected.