Cancel
Showing results for 
Search instead for 
Did you mean: 

batch processing problem?

Experimenter
Experimenter

hello.

i want to export a lot of assemsblys into iges format, all of them in subidirectories inside a main directory. i want to use the "all files in selected directory and subdirectories" but the program doesnt recognise all the files inside the subdirectories. it just says "there isnt any file selected". whats the problem?

 

thanks

4 REPLIES

Re: batch processing problem?

Gears Phenom Gears Phenom
Gears Phenom

@rc213v   a screenshot would be helpful...

 

but as a guess,  make sure the file type selector is set to assys


Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
SE2019 Pre-Production Testing
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7

Re: batch processing problem?

Experimenter
Experimenter

here is the picture

Re: batch processing problem?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@rc213v  Check the option in the lower right. You have it set to Selected Files Only.  Change it to either Selected Folder or Selected Folder and Subfolders.



Ken
Production: SE 2019 MP4, Testing: SE 2020
http://Grundey.blogspot.com

Re: batch processing problem?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @rc213v

 

 

 

the answer of @KennyG exactly would be what I would suggest to do.

 

regards
Wolfgang