Cancel
Showing results for 
Search instead for 
Did you mean: 

batch save as another filetype

Gears Phenom Gears Phenom
Gears Phenom

I've got a bunch of pipe components that we are sending out of house to get cut. We're needing them in a different filetype, and I'm hoping to figure out a way to save them all out as a different file type en masse. Preferably each to a ".IFC" file or if not that, at least each into a iges file. Is there any way to save out part files to a translated filetype in a batch sort of way?

Solid Edge 2019
Windows 7 Professional
Nvidia K2200 & Intel Xeon
"You're doing it wrong"
3 REPLIES 3

Re: batch save as another filetype

Gears Phenom Gears Phenom
Gears Phenom

Nevermind, I figured it out. I forgot the macro that comes packaged with edge. If anyone wants to know what I mean, navigate to the "custom" folder in your Solid Edge program directory. The folder titled "batch" contains the needed .exe file to achieve this.

Solid Edge 2019
Windows 7 Professional
Nvidia K2200 & Intel Xeon
"You're doing it wrong"

Re: batch save as another filetype

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,


but don't forget the standard translation EXE files in the SE program folder.

 

At least there is a SEIGES.exe, a SEINVENTOR.exe, a SEACIS.exe and soome others 

 

They only one I miss with the ST9 is the SESTEP.exe and I'm pretty sure that this was available in ST8

 

 

regards
Wolfgang

Re: batch save as another filetype

Gears Phenom Gears Phenom
Gears Phenom

That's where it would determine the export settings when I do a batch convert?

Solid Edge 2019
Windows 7 Professional
Nvidia K2200 & Intel Xeon
"You're doing it wrong"