Cancel
Showing results for 
Search instead for 
Did you mean: 

block view selection with Excel macro

Experimenter
Experimenter

Hi,

 

I want to make an automated selection of blockviews with a excel macro.

The solidedge 2D drawing contains a lot of blocks with different views. Depending on the configurated system in excel, we want to configurate the right drawing in SolidEdge, with an excel marco.

 

My main questions are: Is this possible?, does sombody have an example or expirience with this?

 

thx

 

Henk

1 REPLY

Re: block view selection with Excel macro

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

If using Free 2D with no maintenance, it is not possible as there is no API.  If using the maintenanced version or full Solid Edge, then it should be possible and I would recommend asking your question in the Solid Edge Developer forum here:  https://community.plm.automation.siemens.com/t5/Solid-Edge-Developer-Forum/bd-p/SEDeveloperForum

 



Ken
Production: ST10 MP9, Testing: SE 2019
http://Grundey.blogspot.com