Cancel
Showing results for 
Search instead for 
Did you mean: 

calculate in parts list table

Phenom
Phenom

Is this possible?

I have a custom property in parts called "quantity". 

This property is filled in the table generated by the "Part list" function.

 

I can add an extra line behind, but now I would like to have the contents to be the sum of the quantity above. 

YyUOTBQ

...........................................................................................................
Solid Edge 2019 & AutoCAD 2020 user
3 REPLIES 3

Re: calculate in parts list table

Honored Contributor
Honored Contributor

I have the same desire, but for the weight.

 

The problem is, formatting of parts list requires all line in the parts list to use the same formatting.

As a result, this can't be added to the parts list it's self.

I use a piece of annotation for this

Highlighted

Betreff: calculate in parts list table

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Joris

Hi @12GAGE

 

 

 

take a look into the BOM option for "Grouping"

 

I can not say 100% wether You can build a sub-total of any numeric values or not, but I know that You can define groups to be build.

 

 

regards
Wolfgang

Betreff: calculate in parts list table

Phenom
Phenom

Thanks for the replies, but I can't find a thing.

 

The problem is (I think) that the quantity is a manual inserted number.

I could work with an excel link, but I don't trust that. To much troubles with that in the past.

...........................................................................................................
Solid Edge 2019 & AutoCAD 2020 user