Cancel
Showing results for 
Search instead for 
Did you mean: 

callout properties date format

Valued Contributor
Valued Contributor

Hello all!

 

I need a little bit of information.

 

In the callout properties box, there is a callout text "%{Created/@MM/dd/yy}"

 

Is there a way that we can change the format to retrieve today's date?

 

Thank  you my friends!

 

7 REPLIES 7

Re: callout properties date format

Honored Contributor
Honored Contributor

%{Modified} will show the date the file was last saved.

Re: callout properties date format

Valued Contributor
Valued Contributor

@12GAGE

 

Way wicked,  copied the text and placed into the box, saved and reopened.

 

TADA!

 

Thank you very much!

 

 

Re: callout properties date format

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I don't believe so, but if you want a date that updates when you open it, you should be able to use:  %{Accessed}

That should update anytime someone opens the file.

 

There is also:  %{Modified}

This will update whenever the file is saved.

 

If you are simply looking for a static date to be generated automatically and don't wish it to change at anytime after that, then I'm afraid you will just need to type it in.



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com

Re: callout properties date format

Valued Contributor
Valued Contributor

@KennyG

 

I tried that one and it gave me the date for yedsterday.

 

Thank you for the information though.  Gonna put that one in my notebook for later use.

 

Got tired of updating all of the dates everytime on every single drawing.

 

Im using this for a more automated response to help take care

Re: callout properties date format

Valued Contributor
Valued Contributor

@KennyG

@12GAGE

 

Is there kinda like a code book or some information that I can use that would be able to help be modify a draft ticket.  I also want to see if I can place the material properties on a draft sheet as well.

 

 

Re: callout properties date format

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Lex-luthor,

 

Depending on how you want to handle the content, or rather, what content you want displayed, in certain instances, will change what is best suited......I have a few saved configurations, for different conditions [part vs. assemblies, etc]

*Saved Settings: make the callout how you want it, then give it a name & Save....done!

 

If you go into the "Property Text" area [indicated in the image] there are options, and they vary, depending on the drop down chosen......have a browse through and you see what is available, which is also dependant on the available model[s].

 

2017-11-02.png

 

2017-11-02 (2).png

 

 

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: callout properties date format

Valued Contributor
Valued Contributor

@SeanCresswell

 

Cool information to know.

 

I got tired of updating all of the drafts and blocks that I get my hands on.  Authur hits my hands late at night and we are not getting along. LOL

 

I didnt think of looking in the small boxes.

 

Thank you very much Sir.