Cancel
Showing results for 
Search instead for 
Did you mean: 

can I apply water property at solid part?

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer
I made simple assembly and assembled.(1 cup and water) and I tried to apply material "water" at the assembly. I have heard it exist. but I can't found that material in physical property list. how can I apply it?
3 REPLIES 3

Re: can I apply water property at solid part?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there,

 

It is normally set at part level....I presume you have modelled the cup & the water separately...?

I have my Solid Edge Options set so that the material properties are selected before I start any part level geometry.

 

ST8_PAR_SEOptions_General_PromptForMaterial.png

 

From the assembly though, there are a couple of options....assuming you have not applied any material to the models already.

On the "Inspect" tab, run the Properties command, and it should prompt to set material fo each model individually, or globally for them all. [depending on your desired outcome].......or, right click over the part itself [or the listing in the pathfinder] and Edit, or Open into the part and double click on the material listing in Pathfinder, the set your material to water.

 

ST8_ASM_EditPart_EditMaterialFromPathfinder.png

 

ST8_ASM_EditPart_EditMaterialFromPathfinder_SEMaterialTable_Water.png

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP7] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Highlighted

Re: can I apply water property at solid part?

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer
oh my, I can't expected that option. Thank you for your perfect answer and good tip! Smiley Happy

Re: can I apply water property at solid part?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Very welcome.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP7] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000