can I edit multiple parts in assembly using single 2D drawing.

Pioneer
Pioneer

If I have one assembly consist of 4 parts and I want to edit all four parts using single 2d drawing, e.g. I want to cut all parts using one circle. Do I have to copy that circle in all four “part files” or can I cut using only one circle in assembly? 

2 REPLIES

you are looking for "assembly driven part features"  or "...

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

you are looking for "assembly driven part features"  or " assembly features" depends on where you want the features to "live".  SE Help should give you everythign you need.  

 

HTH

Matt Johnson
Application Engineer
Ally PLM Solutions
matt.johnson@allyplm.com
http://allyplm.com/

You can use an Assembly Feature... Look in the Pulldown T...

Phenom
Phenom

You can use an Assembly Feature... Look in the Pulldown Tab and under "Features" you'll see the ability to make afeature in the Assembly, or even make similar "holes" in each of the parts.

assembly feature.jpg

 

I hope that helps.

 

Bob