can I use the working environment in ST5 as in older version like V20 where I can preserve the sketc

Experimenter
Experimenter

can I use the working environment in ST5 as in older version like V20 where I can preserve the sketch & when I need to change the part I have to change the sketch which is not possible in ST5

2 REPLIES

Re: can I use the working environment in ST5 as in older version like V20 where I can preserve the s

PLM World Member Genius PLM World Member Genius
PLM World Member Genius

Make sure to work in ordered mode

 

ordered.png

 

Re: can I use the working environment in ST5 as in older version like V20 where I can preserve the s

Esteemed Contributor
Esteemed Contributor
Also, there is a setting in the options to set ordered as the default start up mode.

Thanks,
Ken

Production: ST9 MP10
Testing: ST10 MP3