Cancel
Showing results for 
Search instead for 
Did you mean: 

can someone recommend an "ergonomic wireless mouse"

Builder
Builder

Hello,

I recently lost my mouse to old age. Was very sad.Robot Sad Now I am trying to find a replacement. Discovered I don't like the wheel with a right/left click. And am currently using one that is tethered (wired), not happy. Saw that there are "ergonomic" mice that help with carple tunnel, which I suffer mildly. So long story short...has anyone had experience in SE using this type of mouse? And Accounting has maxed my spending at $60.

 

Thanks for reading! 

17 REPLIES 17

Re: can someone recommend an "ergonomic wireless mouse"

MLombard
Retired

The Logitech M705 I think is a very nice cordless mouse. It holds a charge forever, it seems. I don't remember how much it was or how much I paid for it, but it's a good mouse.

Retired Community Manager for Solid Edge. This account is no longer active.

Re: can someone recommend an "ergonomic wireless mouse"

Siemens Phenom Siemens Phenom
Siemens Phenom

I have the M705 and can concur that this is a good mouse -- at least for me :-)

Re: can someone recommend an "ergonomic wireless mouse"

Honored Contributor
Honored Contributor

I use a Logitech G700. I like it so much I own 5 of them.

Works both wired and wireless. If you run out of battery, just plug it in for a while when using it.

Re: can someone recommend an "ergonomic wireless mouse"

Phenom
Phenom
I'm using Evoluent VerticalMouse 4 but I'm still looking for a better one Smiley Sad

Yasser

Re: can someone recommend an "ergonomic wireless mouse"

Gears Phenom Gears Phenom
Gears Phenom

 I use Kinesis products also. https://www.kinesis-ergo.com

 

You can sometimes find them on Amazon for a bit cheaper than list price through their website.


____________________________________
--Scott Wertel, P.E.

Re: can someone recommend an "ergonomic wireless mouse"

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@swertel, The vertical orientation of the mouse makes a lot of sense.

Edit: The price, on the other hand...

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200

Re: can someone recommend an "ergonomic wireless mouse"

Honored Contributor
Honored Contributor

The foot pedals are cool, I may get a set for home use with my recording studio.

Highlighted

Re: can someone recommend an "ergonomic wireless mouse"

Phenom
Phenom

I used to be in love with a Logitech M1000 mouse. Then they discontinued it and I was buying them on eBay, until they dried up.

 

I now use the Microsoft Sculpt Ergonomic Mouse and for $32 it's the best around. It's large and simple but it allows the user to rest their palm on it without straining the wrist.

 

Bob

Re: can someone recommend an "ergonomic wireless mouse"

Valued Contributor
Valued Contributor

"12GAGE: I use a Logitech G700. I like it so much I own 5 of them."

 

I did laugh reading this.

I have G700 too, but I got 6 of them. Must work at the 2 locations (Office & Home)x Desktop\Laptop\Laptop bag\Spare.

Programing its buttons to about 13 settings, their programmed function can be memorized in short time, clicking them without the thinking and best is that each of these option reads if my ST8  or SolidWorks 2016 Premium is open, so it calls the appropriate function in both CAD programs.

Naturally I did put on the button options the same function for both SE or SW.

This saves a lots of hand travel and it fits OK using the low height of the mouse pad relative to my ergo chair.

 

Milan

www.aaaengineering.com

 

Milan Wendl, MEngSc, P.Eng.
AAA Engineering, Canada
ST10, SolidWorks Premium 2018