Cancel
Showing results for 
Search instead for 
Did you mean: 

change line thickness in Visible Edge display mode (not Draft or drawing)

Is there a way or a config file where I can change the default line thickness on view styles-visible edges?
I know that this can be easily managed in drawings but we use intensively bitmap screenshots and would be nice to increase a bit this oncreen thickness ...

3 REPLIES

Re: change line thickness in Visible Edge display mode (not Draft or drawing)

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Sort of...  You need to modify the Face Styles you are going to use and there is an Edges - Width setting, HOWEVER this only applies to hard edges and not horizon edges so unless your part is strictly a flat face faceted part, it will look like a hybrid with thin lines for the horizon edges and thicker lines on the hard edges.

2015-12-18_15-40-52.png



Ken

Production: ST10 MP7
Testing: SE 2019
http://Grundey.blogspot.com

Re: change line thickness in Visible Edge display mode (not Draft or drawing)

Thanks Ken but the things we design are mainly having horizon edges...

so it does not solve fully.
There may be a parameter somewhere, but it might ne hard-coded in the source.

Re: change line thickness in Visible Edge display mode (not Draft or drawing)

Well, so far the best way we've found is to edit the Saved Image from the active view in PhotoShop, using the minimum filter.
Of course there is no association and if the design changes than the process must be repeated...