Cancel
Showing results for 
Search instead for 
Did you mean: 

changing centre of rotation

Valued Contributor
Valued Contributor

how can i change the centre of rotation.

 

in the past i have noticed unintentionally i have done this where a pink line or dot is placed on the model, this changes the rotation. 

 

how can i toggle this on and off?

 

 

Regards,

MagRiz
(ST9 User Est 01.18)
2 REPLIES 2

Re: changing centre of rotation

Siemens Phenom Siemens Phenom
Siemens Phenom

@MagRiz  In the rotate command, when you locate and click on a point or linear edge that point or edge becomes the center point or axis of rotation. I am not aware of a way to disable this.

 

Greg

Re: changing centre of rotation

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

@MagRiz  You can try middle-mouse-clicking or clicking the wheel in an empty space in the model.