Cancel
Showing results for 
Search instead for 
Did you mean: 

construct a cover for a cilinder cut

Pioneer
Pioneer

How can i construct a cover for a cilinder cut?

The cover must fit into the tube or up to the cut surface

cover.jpg

3 REPLIES

Re: construct a cover for a cilinder cut

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @KurtCouffez,

 

There are a couple of ways to go about this......the most logical way I find is....model the pipe [which you have done] you can insert a part copy of the pipe into a new sheet metal file, to then make single line contour flange to cover the beveled end of the pipe, then making a normal cutout to trim away outwards from the ID of the pipe.  Done!

 

See my example ST8 files as attached.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP4] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: construct a cover for a cilinder cut

Pioneer
Pioneer

Thx, this will do it.

Re: construct a cover for a cilinder cut

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

No worries......any time.

 

Happy Edging. Robot Happy

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP4] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000