Cancel
Showing results for 
Search instead for 
Did you mean: 

conversion Part Size

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

I want to know reducing a part(or Assembly)'s entire size at once. how can I do it?

 

-------------------------------------------------------------

 

+added

 

When I test Wire Harness Module, I have faced some problem.

 

the problem is bluedots, In Wire Harness environment.

 

 

I tried to move the bluedots, but It just operated mouse dragging.

 

1 REPLY 1
Highlighted

Re: conversion Part Size

Valued Contributor
Valued Contributor

Create a new part file.  In this blank part file in the Home tab, select Part Copy.

 

Part Copy.jpg

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

Then select either the Part or Assembly you would like to scale.  

 

Part Copy Parameters.jpg

 

Now you can scale in the X, Y, and/or Z direction.  Numbers greater than 1 make the part larger.  Between 0 and less than 1 make the part smaller.  You can also select Shrink Factor, in this case, numbers larger than 1 make the part smaller and numbers between 0 and less than 1 make the part larger.

 

If you want to keep the assembly as an assembly file, you may need to save your assembly with a new name, scale each compoenent individually, save each as a new part, then replace each compoenent in the assembly with the new parts.  

Brian Fritz
Solid Edge Certified Professional
ST8 latest MP