Cancel
Showing results for 
Search instead for 
Did you mean: 

coordinates on drawing

Valued Contributor
Valued Contributor

Version 106.00.05.04x64

Hello,

is it possible to display the coordinate system (X,Y,Z) on the drawing view? Not the center of mass, but just X Y Z axes

This doesn't work...

Display a coordinate system in a drawing view

A selected coordinate system can be displayed in the drawing view by doing the following on the Display tab (Drawing View Properties dialog box):

  1. Select the Parts List Options button, and then select List Coordinate Systems.

  2. From the Parts list, select the coordinate system you want to show.

  3. Select the Show check box under Selected Part(s) Display.

  4. From the Visible edge style list, select the line style for displaying the coordinate system.

  5. Click Apply.

3 REPLIES 3

Re: coordinates on drawing

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Hello Johan,

 

I tried the workflow you listed and found that additionally updating the view displays the coordinate system though it is very difficult to view since it appears as a small dot as shown below:

p.png

There sure must be setting, which I have not been able to locate, that makes the coordinate system appear properly the way it looks like in the Part.

 

If you know or discover the setting, kindly do share it here.

Re: coordinates on drawing

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

Yes, Tushar is right. You will see a "very" small dot, but there are some ways to show it in larger. You have to create a new line style or you have to create sketches in 3D and show them on drawing view. Solid Edge ST7 will provide a great new way to show coordinate system...

 

Here is a video about solutions in ST6 and ST7:

 

 

I hope, this will help!

 

BR,

Imics
http://solidedgest.wordpress.com/

Re: coordinates on drawing

Valued Contributor
Valued Contributor

thx for the replies, but as i  understand very poor feature in today SE version