Cancel
Showing results for 
Search instead for 
Did you mean: 

could someone tell me how to install the PDF printer please as I need to export on this format

Creator
Creator

as a new user i wanted to export in a PDF format, but the option is not listed in the Options of the save as dialog

could you help please?

 

For info

when i open the save as/translation option, i am give the chice of

.dwg

.dgn

.dxf

.sev

incedently i am using windows 8.1 x64. is this an issue?

 

thank you

11 REPLIES

It should be there. look for Save As Translated --> Adobe...

Community Manager Community Manager
Community Manager

It should be there. look for Save As Translated --> Adobe Acrobat Documents or Adobe Acrobat 3D Documents.

Dan Staples
Director, Solid Edge Product Development

Re: It should be there. look for Save As Translated --> Adobe...

Creator
Creator
Hi

Thanks for the quick reply

When i look in Saveas/translate the options i have are

.dgn

.dwg

.dxf

.sev

Incidentally i am running Windows 8.1 64bit [if that makes a difference]



Roger

Re: It should be there. look for Save As Translated --> Adobe...

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

So this is only from draft?,...or are you not seeing the Save As *PDF & *3D PDF in the model environments either?

SE_ST6_File_SaveAs_Translated [dft].png

 

SE_ST6_File_SaveAs_Translated [par, psm, asm].png

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP4] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: It should be there. look for Save As Translated --> Adobe...

Phenom
Phenom
Before we go digging around can you confirm one thing for me? Your original question says "export in PDF format". I would like to confirm that "export in" does NOT mean that you are looking to open a pdf in Solid Edge.
Also that you are using Windows 8.1 and not Windows 8?

Re: It should be there. look for Save As Translated --> Adobe...

Creator
Creator
Hi

Once again thank you for your reply.

My first answer regarding PDF is that I need to export pdf files from Solid
Edge.

The second answer is that I can confirm my operating system is Windows 8.1
and is the 64 bit version

Thanks

roger

Roger. time for a screen shot from you or log an IR. this...

Community Manager Community Manager
Community Manager

Roger. time for a screen shot from you or log an IR. this is too mysterious to figure out in words only on a discussion forum.

 

Dan Staples
Director, Solid Edge Product Development

What version of Solid Edge are you running? STx?

Community Manager Community Manager
Community Manager

What version of Solid Edge are you running? STx?

Dan Staples
Director, Solid Edge Product Development

Re: Roger. time for a screen shot from you or log an IR. this...

Creator
Creator
Sound complicated

What do i have to do?

Re: What version of Solid Edge are you running? STx?

Creator
Creator
ST6 Free version 2D