Cancel
Showing results for 
Search instead for 
Did you mean: 

creating a cam

Pioneer
Pioneer

I want to create a cam in SE ST10 as shown in the youtube link:

https://youtu.be/t9wTZrV-GL4

How do I do this in SE?

Thanks for any help

Walter

 

Walter ST10 mp11 Win 7 Ultimate
Quadro k4200
5 REPLIES

Re: creating a cam

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @wbrokow1,

 

Almost the exact same way.....just the command terminology is different.

 

Something like....

  • Create extruded cylinder
  • Create profile sketch, on tangent plane
  • Wrap sketch command
  • Normal cutout

 

Rough 20 second example file attached.....

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP3] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: creating a cam

Pioneer
Pioneer

great thank you . I will give it a try soon.

 

 

Walter ST10 mp11 Win 7 Ultimate
Quadro k4200

Re: creating a cam

Pioneer
Pioneer

How canyouuse a formula likethe guy in the video.

for example if x is the diameter of the cylinder.for the lenght of theline I can put l=x*pi.

Where l is the length of the flat sketch line that's equalto the circumference of the clinder.

Thanks for any help

Walter ST10 mp11 Win 7 Ultimate
Quadro k4200

Re: creating a cam

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @wbrokow1

 

 

without having watched the files, but defining a formular rule for any variable is done in the variable table within the formular field.

 

Or do a double click onto the dimension what also will open the dims variable form for You.

regards
Wolfgang

Re: creating a cam

Pioneer
Pioneer

thanks i will give it a try

Walter

Walter ST10 mp11 Win 7 Ultimate
Quadro k4200