Cancel
Showing results for 
Search instead for 
Did you mean: 

dft corrupted file

Creator
Creator

Is there some way or tool to fix a dft corrupted file? (I was working with this file, I saved it, I closed it, then I tried to open it and SE could not open the file.)

 

st5 dft error.jpg

 

3 REPLIES

There is no tool, but if you have a Maintenance agreement...

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

There is no tool, but if you have a Maintenance agreement, you can submit it to GTAC either directly or through your VAR to possibly get it fixed if it is worth the wait of a few days to do so.



Ken
Production: ST10 MP9, Testing: SE 2019
http://Grundey.blogspot.com

Re: dft corrupted file

Experimenter
Experimenter

As far as I am concerned, you are able to download Data Recovery and have a try. It is a very useful program. WIth this software, you can restore corrupted files as soon as possible.

Re: dft corrupted file

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@flx  I assume you did the basics first?  Hard reboot, restart SE and see if it opens.

You could try going to file properties and select the tab "previous versions" and see if there are any previous saved versions.

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200