Cancel
Showing results for 
Search instead for 
Did you mean: 

drawing wiring diagram

Experimenter
Experimenter

Hello,

 

is it possible to draw wiring diagrams with solid edge 2D Drafting with lines wich are connected to the desired components and following dynamically while moving the components.

 

Thanks for a quick answer!

 

Schweppes

 

1 REPLY 1

Re: drawing wiring diagram

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Yes.  Solid Edge comes with an electrical Block library or you can use your own to place your electrcal symbols, and then you you can create the circuits with the "Connector" command which will provide you with the behaviour that you are asking for.  The Connector command is found on the "Home" ribbon tab in the "Annotation" section, or you can use the Command Finder at the bottom of your screen to find it.



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com