Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

dxf to sketch

Valued Contributor
Valued Contributor

Hello forum!

 

I have a thought that needs pondering.

 

I have several dxf files that work really well in draft sight. 

 

I need to create cutout templates for each of the dxf files.  51 files total

 

Is there a process to create sketches from those dxf files and if so how?

 

Thank you for your time and input.

 

10 REPLIES 10

Betreff: dxf to sketch

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Lex-luthor

 

 

I think first approach can be a simple "Copy/Paste" procedure or You use the 3D Create from draft

 

Keep in mind, that You can open a DXF directly as sketch within a part/asm

 

 

regards
Wolfgang

Re: dxf to sketch

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @Lex-luthor,

 

If you are looking to set these profiles up for easy re-use after importing into Solid Edge, then I would look at setting up a block library [works in 2D Draft's ony] for them.....or else if you need profiles for 3D use, then set up a feature library.

 

ST10_DFT_CopyToLibrary.png

 

As @hawcad points out, Copy/Paste is a simple way to transfer geometry from one file to another.....you may want to check the 2D Paist Behaivior in SE-Options, is how you want it to happen.

 

ST10_SEOptions_General-2DPaisteBehavior.png

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP5] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Betreff: dxf to sketch

Valued Contributor
Valued Contributor

@hawcad

 

Its gonna take me a little time to play with the files. 

 

When I ty to open the dxf as a part, there is nothing there.  I am using SE ST9, ordered level.

 

Thank you for the quick replay though

 

Betreff: dxf to sketch

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Lex-luthor,

 

DXF files are [as far as Solid Edge is concerned] 2D only files, so you will need to open them into a DRAFT template first, then you may copy/paste your geometry into PAR, or PSM profile sketch.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP5] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Betreff: dxf to sketch

Valued Contributor
Valued Contributor

@SeanCresswell

 

Sounds like Im gonna be in for some fun!

 

Thank you Sean!

 

 

Betreff: dxf to sketch

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Actually DXF files can be opened directly to a Part Sketch.  When using the SE Open form, select your DXF file with a single mouse click and then select the 2017-10-02_15-23-35.png button.  You should see a selection like the pic below where you can decide how the DXF file is opened.

 

 



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Betreff: dxf to sketch

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Oh yeah, forgot that "option" was there........that'll get @Lex-luthor what is required much faster.

 

However, I do wish the user didn't HAVE to use this method. Choosing what template [PAR, PSM, ASM, DFT] "should" run the options allowed [user defined] for that selection, in order to achieve the same import.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP5] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Betreff: dxf to sketch

Valued Contributor
Valued Contributor

@SeanCresswell

 

Took me a few mins and a few hundred tries, but I managed to finally get it through, now just have to scale it down to the correct size, it is like 100 fold bigger than what I thought.

 

Again, Thank you Sean.

 

 

Betreff: dxf to sketch

Phenom
Phenom

As you step through the Options you should see a converesion units setting. make sure you have that set correctly.

The usual case is to be 2.54 or 25.4 out - inches to/from mm.

HP Z420 16GB RAM
Quadro K4000
SE2019 MP5 on Windows 10 Pro 64.