Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: edit link in draft

Valued Contributor
Valued Contributor

I will try restarting SE....back in a few minutes...

Re: edit link in draft

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Greybarn,

 

I use this same procedure, from time to time also....but have not encountered this broken links to the views, after performing edit links. Sometimes, if I have manipulated the view frame, the new part is out of sight, until frame is dragged to show the part....but I don't think that is your issue.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: edit link in draft

Valued Contributor
Valued Contributor

Rebooting did not do anything.

How do I upload multiple files?

Highlighted

Re: edit link in draft

Valued Contributor
Valued Contributor

Here is a zipped file with the original Draft, the original assembly, and the new assembly that is trying to use.

Let me know if you see anything weird.

Regards

Peter

Re: edit link in draft

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Greybarn, Foiled by differing SE versions. We're still on ST9. Maybe someone on ST10 will give it a go.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: edit link in draft

Phenom
Phenom

@Greybarn I am seeing the same thing as you are with the dashed lines when I rename the drawing and change link to the other assembly. I don't have time at the moment to look closer at it, but I may be able to look into it later today or tomrrow.

 

Bob Henry
REH Technical Consulting
Canonsburg, PA 15317