Cancel
Showing results for 
Search instead for 
Did you mean: 

editing flanges

Valued Contributor
Valued Contributor

Most of the videos that I have seen only show on how to create different flanges from edges and more flanges from that as different contour edges.

 

the problem that I have been comming across is that when I am working within my sheet metal, The flange that I need is typically shorter than the entire edge of the sheetmetal.

 

ergo; 20 inch edge and I need only a 11 inch flange with an outside metal bend.

 

Is there a instruction on hos to do this?

 

Thank you so very much!

 

 

5 REPLIES 5

Betreff: editing flanges

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Lex-luthor

 

 

 

 

there are several way to achieve this, depending on wether You are in Ordered or Synchronous

 

In ordered mode You have the option tabs when creating the flange/contour flange

 

In sync, You also have one option for complete edge or partial edge (not mor as in ordered)

And You also can move the side face of any flange afterwards using the steering wheel.

 

 

regards
Wolfgang

Betreff: editing flanges

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Lex-luthor

 

 

and here is the video as attached ZIP

 

 

and @bshand

 

there are several posts regarding the issue with the video attachments.

I think this is a major forum problem 

regards
Wolfgang

Betreff: editing flanges

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Thanks @hawcad. Haven't been on the forum much lately.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Betreff: editing flanges

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @bshand

 

 

 

no problem.

 

Here is the link to that posts:

 

https://community.plm.automation.siemens.com/t5/Solid-Edge-Forum/Error-message-displayed-viewing-a-p...

 

 

regards
Wolfgang

Betreff: editing flanges

Valued Contributor
Valued Contributor

I always work in ordered since it is sheetmetal parts and thank you very much for video.  That helped a great deal and explained alot of things.