Cancel
Showing results for 
Search instead for 
Did you mean: 

editing swept protrusions

Pioneer
Pioneer

Hello Experts,

 

I was wondering how a Swept Protusion can be modified after it is created. I clicked on it once and twice but neither open the dialog box to edit.

 

I appreciate your help.

4 REPLIES

Re: editing swept protrusions

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

If done in Synch, you really can't edit it.  Those kind of features need to be done in Ordered so that you can edit the input sketches for path/cross section.



Ken
Production: ST10 MP7, Testing: SE 2019
http://Grundey.blogspot.com

Re: editing swept protrusions

Pioneer
Pioneer

IC. Thanks for your reply. It helped a lot.

Re: editing swept protrusions

Phenom
Phenom

This is exactly what the Live Section command is for in Synch. This will allow you to cut the sweep anywhere you want, and will create a linked cross section that you can then adjust.

 

Capture.PNG

-Dylan Gondyke

Re: editing swept protrusions

Pioneer
Pioneer

Thanks Dylan. It is a good point. However, after I created the Live Section, I could not make modifications, I think because of relationships. I need to work on that more.