engeneering reference

Experimenter
Experimenter

sorry
I just installed the solid edge st6 and I can not access engeneering reference, I can do to enable this option, as it comes off in the program
Thank you.

 

5 REPLIES

Davrick   I believe you have to install Standard Parts, w...

Phenom
Phenom

Davrick

 

I believe you have to install Standard Parts, which requires a separate installation. Should be on your DVD. But I also think you need to have Solid Edge classic to have STD. Parts.

 

Update. i just checked and it's on the distribution DVD.

 

dvd.png

On your Solid Edge ST6 DVD there should be a folder entit...

PLM World Member Experimenter PLM World Member Experimenter
PLM World Member Experimenter

On your Solid Edge ST6 DVD there should be a folder entitled Engineering Reference.  Open this folder and run the Setup.exe program and go through the prompts.  After you have run the program with Solid Edge closed.  If you open Solid Edge your Engineering Reference should then be available.

Thanks,
Nate Emler
Engineering Programmer
Ariel Corporation

Re: On your Solid Edge ST6 DVD there should be a folder entit...

Experimenter
Experimenter
and hise that but does not appear available, aparese idle but when I look in the control panel is installed the program and the Engineering Reference

Re: On your Solid Edge ST6 DVD there should be a folder entit...

Esteemed Contributor
Esteemed Contributor
What license do you have (classic, premium, design & drafting)?
Also, it is active in the Assembly environment only as an Edge Bar pane.

Thanks,
Ken

Production: ST9 MP10
Testing: ST10 MP3

Re: Davrick I believe you have to install Standard Parts, w...

Experimenter
Experimenter

Hi! I have the same problem but I have academic version (so I have no DVD). Could you please help me, which file should I open to get that screen you mentioned?