Cancel
Showing results for 
Search instead for 
Did you mean: 

export draft as PDF with layers in it

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

I have a draft with different layers in Solid Edge and want to export these draft as a PDF format with all the layers in it. because in the Acrobat reader, I want to have the possibility that i can hide or unhiden the layers.

this is not possible in Solid Edge, have anyone expirience with a work around or a free viewer that shows the layers?

because, even the SE viewer don't show the layers.

any suggestions is welcome.

 

4 REPLIES

Re: export draft as PDF with layers in it

Phenom
Phenom

A workaround, though it's not great, is to export as a DXF, then from AutoCAD, DraftSight or similar, export a PDF including the layers.

Another PDF viewer isn't going to help as the layers aren't there to view, not sure about other SE draft file viewers.

Re: export draft as PDF with layers in it

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Right, Solid Edge does not appear to save layer information in the exported PDF.

Good workaround Alex_H !!

 

~Tushar

Re: export draft as PDF with layers in it

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Ask and ye shal be enhanced.

Your recent call to the Global Technical Access Center, Incident Report (IR)Number 7534090 opened on 14-OCT-2015, has been researched by our GTACsoftware engineers. They have determined that this issue should be  reviewed for possible enhancement to the current software functionality.

LMGi
www.TLMGi.com

Re: export draft as PDF with layers in it

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

BRILLIANT!.....thanks for the update @JasonTitcomb

 

TBH, I hadn't even realised it didn't export them....further, it would be good if there was also an option in that enhancement, to flatten the layer structure, incase of sensitive layer names, that might give away too much info.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP8] Classic [x3 seats]
Windows 10 - Quadro P2000
Testing: Solid Edge 2019