Cancel
Showing results for 
Search instead for 
Did you mean: 

falha do st7 no w10

Experimenter
Experimenter

 como tenho que proceder ,o st7 abre e na mesma hora ja aparece uma janela com mensagem!

3 REPLIES

Re: falha do st7 no w10

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there,

 

You need to have maintenance pack 4, or later installed to run ST7 on Windows 10.

Ideally, and especially if running Student Edition, you should install ST8.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP8] Classic [x3 seats]
Windows 10 - Quadro P2000
Testing: Solid Edge 2019

Re: falha do st7 no w10

Experimenter
Experimenter

obrigado,mas na universidade so usam o st7 e cria incopatilidade,como faco para baixar mpack 4ou posterior para o  w10 ou st7 ,o st7 nao me da tempo de abrir nada e fazer uma atualização.

Re: falha do st7 no w10

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,

 

Problem lies in that Windows-10 was officially released well after ST7.

I'm confused,...so the school has made the upgrade to Win10, then it seems a bit silly to leave application like Solid Edge on an older version also. Especially when it is also free to do so.

 

ST8 will run on the same computer system as one that was previously running ST7. I'm not sure what the incompatibility issue could be in relation to.....I have heard no reports of anything specific to this combination.

 

Maybe you could upload your crash log file here, and someone could take a look.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP8] Classic [x3 seats]
Windows 10 - Quadro P2000
Testing: Solid Edge 2019