Cancel
Showing results for 
Search instead for 
Did you mean: 

find hole sizes in all parts in a folder?

Legend
Legend

I'm probably asking for something that isn't available, but thought I'd ask before doing it the hard way...............

 

I have a folder that has 2-300 sheet metal parts, and I'm needing to find which ones have a specific hole size in the parts. I thought property manager might do it, but seems not. Am I stuck with opening each file and seeing what size holes it has?

4 REPLIES 4

Betreff: find hole sizes in all parts in a folder?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Trikefreak 

 

 

 

 

I think, and that's the bad answer, this only will be possible with an API macro, or modification in the batch macro of the custom example folder.

 

 

regards
Wolfgang

Re: find hole sizes in all parts in a folder?

Gears Phenom Gears Phenom
Gears Phenom

@Trikefreak I'd suggest reaching out to someone in the Developers Form and ask if you could get some assistance.

Matt Johnson
Solid Edge Certified Professional
Solid Edge 2019 (SEEC) - Production
NX12 (Tc Integration)
Teamcenter 10.1.7

Betreff: find hole sizes in all parts in a folder?

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

@hawcad wrote:

 

I think, and that's the bad answer, this only will be possible with an API macro, or modification in the batch macro of the custom example folder.


I agree, only a custom or customized batch processor can do this job.

Betreff: find hole sizes in all parts in a folder?

Legend
Legend

That's a bummer. It would be cool to be able to view something similar to Family of Parts table, and view a folder with all that information........(hint, hint, to Siemens folks peeking around).