Cancel
Showing results for 
Search instead for 
Did you mean: 

find the original part that was used as the "save as" on the part i have now

Creator
Creator

how can i find the original part that was used as the "save as" on the part i have now

3 REPLIES 3

Re: find the original part that was used as the "save as" on the part i have now

Phenom
Phenom

if nobody has modified already, you can look in the file properties, see if the original document number is there.

Re: find the original part that was used as the "save as" on the part i have now

Creator
Creator

yes i tried that and dont see any where in the file properties list where it would show the original part.

 

Re: find the original part that was used as the "save as" on the part i have now

Gears Phenom Gears Phenom
Gears Phenom

@billyhill  Nothing at all that it could share in common with the original? Nothing in the Title: Manager: Company: Category: Keywords: Comments: etc. which have possibly remained the same as the original which you could then use as the basis for a search?

Solid Edge 2019
Windows 7 Professional
Nvidia K2200 & Intel Xeon
"You're doing it wrong"