Cancel
Showing results for 
Search instead for 
Did you mean: 

gdiplus.dll installation error

Solution Partner Genius Solution Partner Genius
Solution Partner Genius


Hello everybody!


When I try to install SOLID EDGE, appear message like as below,

"The program can't start because gdiplus.dll is missing from your computer"

How can I solve this problem?


Thank you!

7 REPLIES

Re: gdiplus.dll installation error

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@LittleWillie76,

 

You might need to explain your version of Windows, and the version of Solid Edge you're trying to install, in order to get proper feedback on a solution for this....but is potentially an compatibility issue.

 

Have you tried looking it up on Google?....I found this link  to an old Microsoft forum post, that might be of help.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP4] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: gdiplus.dll installation error

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Thanks to your attention for this issue!

 

I get knew that gdiplus.dll install error is relate with MicroSoft software.

 

So, I'll try to solve this issue with your advice.

 

Thank you!

 

Best Regards.

LittleWillie76

Re: gdiplus.dll installation error

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@LittleWillie76 What version of Solid Edge on what version of Windows?



Ken
Production: ST10 MP9, Testing: SE 2019
http://Grundey.blogspot.com

Re: gdiplus.dll installation error

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Thanks to your attention for my issue.

 

It is ST8, and Win7 Pro 64bit.

 

 

Regards

LittleWillie76

Re: gdiplus.dll installation error

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

OK, thanks for that.  All supported so that is good.

 

gdiplus.dll is related to graphics so I would apply the latest driver for your graphics system in your PC which may resolve the issue.



Ken
Production: ST10 MP9, Testing: SE 2019
http://Grundey.blogspot.com

Re: gdiplus.dll installation error

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

If the graphics driver does not repair the issue, the following should resolve it...

 


Click Start
Type: CMD, from the results, right click CMD
Click 'Run as Administrator'
At the Command Prompt, type: sfc/scannow

This will check for any integrity violations

Restart your system

1. Insert the Windows 7 DVD
2. Restart your computer
3. When asked if you want to boot from your DVD drive, do so.
4. Choose your language, click Next.
5. Click 'Repair your computer'
6. Select operating system you want to repair.



Ken
Production: ST10 MP9, Testing: SE 2019
http://Grundey.blogspot.com

Re: gdiplus.dll installation error

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Thank you!

 

I will try to solve this issue according to your advice.

 

And I'll let you know the result.

 

Regards

LittleWillie76