how can i make the link in solid edge to nx 8.5 cam?

Experimenter
Experimenter
How can I place a button in Solid Edge ST5 so that I can link de partfile to NX 8.5?
3 REPLIES

The button should already be there. On the "Tools" tab lo...

Community Manager Community Manager
Community Manager

The button should already be there. On the "Tools" tab look for CAM Express (rightmost on the tab). This should launch with the current Solid Edge file.

Dan Staples
Director, Solid Edge Product Development

Re: The button should already be there. On the "Tools" tab lo...

Pioneer
Pioneer

what is the cause when the button is greyed out?

But the software is actually loaded on the computer.

Re: The button should already be there. On the "Tools" tab lo...

Pioneer
Pioneer

Answer from John PEarson from Designfusion;

Hi Bruce:

 

This usually happens automatically, but if not you have to manually register the nxcam_dll.

 

To do this close SE and  open a command prompt window.

 

Change your directory to the NX main directory. For you that should be C:\Program Files\Siemens\NX 9.0\UGII.

 

Then type in the following command:  regsvr32 nxcam_64.dll and hit enter.

 

You should get a message window saying that this was successful. Now open SE and see if the icon is active.