Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

how do I change the template of a completed drawing?

Experimenter
Experimenter

is it possible to change the template in a drawing that is complete?

I have customer drawings that need a different tolerance block and

customer name. its very tedious to manually change each one.

7 REPLIES 7

It is not possible to change the template, but you can ch...

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

It is not possible to change the template, but you can change some of the elements of the drawing template depending on how it was set up.  For instance, if you set up your 'customer name' as a draft file property and placed it on your title block using Property Text, then a simple edit of the property is all that is needed.  Simialarly a tolerance block could be set up the same way or if it was placed on the background sheet, you could just edit it in the background sheet and it would then update on all sheets that used the background.

 

Templates are what I call a 'seed' file.  They are simply opened when you create a new file and then a 'Save As' is performed to create the new file.  After that, all you can do is change the content of the files you have created from it.  The key is to strategically set up the stuff you may have to frequently change using the tools in Solid Edge that enable rapid change such as Property Text.



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: It is not possible to change the template, but you can ch...

Experimenter
Experimenter
thanks, was hoping someone smarter than myself had a trick. seems like
a pretty common problem when your company gets sold and the new
owners want their name and drafting standards on the product drawings.

Re: It is not possible to change the template, but you can ch...

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
In your original post, it sounded like this was a limited thing. The following application link will replace the background sheet contents in bulk... Don't know about it much. The author is German but the macro can be ran in English. http://www.incobase.de/download_soft/CBSheets_V1025.zip


Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

One way that I have accomplished something similar is to...

Theorist
Theorist

One way that I have accomplished something similar is to turn off the working sheet and turn on the background sheet. (View Tab) then delete the title block from the drawing you want to copy to. And then turn on the background and turn off the working on the template file and copy the whole drawing template to the background of the new drawing.Then turn off the background and turn on the working sheet and voila. ..hopefully that makes sense. NOTE: This will only work if the two drawing templates are the same size (ie 2 B sized drawing files)

Ben

Re: It is not possible to change the template, but you can ch...

Pioneer
Pioneer

Hi @KennyG, thanks for the clear explanation.

 

Would you happen to know if this still applies to SE 2019?

 

It seems like such a common and basic problem, with high impact for many users in terms of time. I would expect this to be a relatively simple issue for the Solid Edge software development team to fix.

Re: It is not possible to change the template, but you can ch...

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@DvG  If you are referring to replacing templates, a command was added in ST9 or ST10 I believe called "Replace Background" which is ran from a Background sheet and allows specifying another file and then selection of a Background Sheet in that file to replace the the current Background with.  It is not a batch edit tool as you must open files one by one to replace their backgrounds.  If batch change is required you must use a custom macro to do this.

 

In the Custom folder under the Solid Edge instalation directory, there is a sample Batch macro that will convert files into other formats.  It includes the source code so that you can customize it to do other things.  Otherwise you will need to find an existing macro to do this from a VAR or other user such as the one mentioned in a previous post.



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: It is not possible to change the template, but you can ch...

Pioneer
Pioneer

@KennyG, Thank you very much. I will have a look at that.