Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

how do i place a degree symbol in the parts list in a draft drawing

Builder
Builder

how do i place a degree symbol in the parts list in a draft drawing?

2 REPLIES 2

ALT+0176 °

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

ALT+0176 °



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Hi there,   If I understand what your wanting to do here...

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there,

 

If I understand what your wanting to do here correctly....

 

You're wanting to add it to the description of the auto populated field[s] in the parts list, or BOM......in the Parts List Properties > Data tab...you can right click on the cell, and choose "Allow Cell Overrides", then double click to append with the "%DG" short code for the degree symbol, placed where you want.

 

SE_ST6_Draft_PartsListProperties_Data_AllowCellOverrides.jpg

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP7] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000