Cancel
Showing results for 
Search instead for 
Did you mean: 

how do you add a material in st8?

Experimenter
Experimenter

i knew how to do it my older copy (ST8) now i cant seem to figure out how?

3 REPLIES 3

Re: how do you add a material in st8?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there,

 

If you right click on an entry, you get an option to add new material, then fill out all the relevant spec you want for that.....else, just select copy & paste it to the folder you want, then rename it accordingly.

 

FYI: fast way to get to Material Table...."double click" the Material listing in the Pathfinder. [if you don't already have the "Prompt for material...." checked in SE-Options]

 

2015-11-13 (2).png

 

 

I do hope developement update the material table dialogue, to be able to reorder the material listings, on the fly.....without the need to modify it externally in Excel.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Highlighted

Re: how do you add a material in st8?

PLM World Member Genius PLM World Member Genius
PLM World Member Genius

1.Open the material table in Solid Edge

2.Right click on the category you wish to add the new material to

3.Name the material and assign its properties

4.Click Save at the bottom

 

However, if you want to do lots of modifications or a large cleanout...

 

1. Right click the name of your material table at the top of the tree

2. Click Save as

3. Save as an .xls or .xlsx file

4. Edit in excel per the instructions

5. Right click the name of your material table

6. Click import and select the file

 

 

Shane Murray
SE2019 MP6

Re: how do you add a material in st8?

Legend
Legend

Whatever happened to the matweb intergration into solidedge?