Cancel
Showing results for 
Search instead for 
Did you mean: 

how do you create an axis?

Valued Contributor
Valued Contributor

im trying use the feature 'coincident by axis' to create a plane. but i dont have an axis. 

how do i create one?

 

i want the axis to be the centre axis of a cylinder.

Regards,

MagRiz
(ST9 User Est 01.18)
3 REPLIES

Re: how do you create an axis?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

It doesn't mean that you need an axis like through the middle of cylinder. It allows you to determine the X/Y orientation. So you pick a plane, then you pick an axis to align X/Y in that new plane. So that would be another plane or a straight edge or planar face, etc.

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Re: how do you create an axis?

Valued Contributor
Valued Contributor
oh, im in SW mind set Smiley Very Happy
Regards,

MagRiz
(ST9 User Est 01.18)

Re: how do you create an axis?

Phenom
Phenom

@MagRiz wrote:
oh, im in SW mind set Smiley Very Happy

 

@MagRiz  Oh dear. I am so sorry. We didn't know.....

Solid Edge 2019
Windows 7 Professional
Nvidia K2200 & Intel Xeon
"You're doing it wrong"