Cancel
Showing results for 
Search instead for 
Did you mean: 

how do you deal with purchased assemblies?

how do you deal with purchased assemblies to make them act as parts.

 

in some cases (ie: bearings) we dumb them down to parts.

 

in other cases we turn them into a weldment.

 

we simply wnat to only ever see this item in a BOM as a part.

 

Is there another method more commnly used?

 

5 REPLIES

Re: how do you deal with purchased assemblies?

Gears Phenom Gears Phenom
Gears Phenom

My Friend,

 

I suggest using purchased assemblies importing in part environment as a multibody part. It has a lot of advantages...

 

For example:

  • easy to handle this "assy"
  • you can use simplified part for "assy"
  • you have control over hatching in draft
  • you can handle "assy" as a part in BOM
  • ... etc

Here is a video, what can be useful:

 

BR,

 

 

Imics
http://solidedgest.wordpress.com/

Re: how do you deal with purchased assemblies?

Genius
Genius

I agree with Imics, it's the best way even though the multibodies can be anoying to look at...

Re: how do you deal with purchased assemblies?

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

From within the purchased assembly you could set all of the components Occurrence Properties to not show in Parts List.

LMGi
www.TLMGi.com

Re: how do you deal with purchased assemblies?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I typically use import part copy and delete unneeded detail (which is usually pretty easy with synchronous) in most cases IF you want to treat that supplied assembly as a single item so that assemblies aren't cluttered with unnecessary faces and graphical overhead and drawings aren't also cluttered with useless detail.

Imic's motor is the type of part we use but we would only be interested in shaft size and location, overall size and mounting base and holes. So the cooling fins for instance would be the first to go among other things. The attached is a representative example.

Bruce Shand
ST10 MP7 - Insight - Win10 - K4200

Re: how do you deal with purchased assemblies?

thanks all,

 

I must have been brain dead...  Multi Body part just was too obvious... 

 

thanks Imre!