Cancel
Showing results for 
Search instead for 
Did you mean: 

how do you sketh this punch?

Creator
Creator

can anyone please tell me?

19 REPLIES

Re: how do you sketh this punch?

Experimenter
Experimenter

Try to use the "Gusset" command under the dimple command in sheet metal,

make the bend first and then use this command, point at the inner radius of the bend

then you can place the "gusset" where you like, You can even choose parameters for the gusset.

Re: how do you sketh this punch?

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Not  a sheetmetal expert even remotely, but looks like a gusset:

 

 

2016June1001.jpg

Re: how do you sketh this punch?

Creator
Creator

Great thanks.

Re: how do you sketh this punch?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Aviad If a someone provided a solution to your question, would you mind marking their reply as the Solution?  This will help future community members when searching for an aswer to the same question.

 

Thanks.



Ken
Production: SE 2019 MP4, Testing: SE 2020
http://Grundey.blogspot.com

Re: how do you sketh this punch?

Creator
Creator

Tushar gave me a good solituon.

I used the gusset function under the dumple feature.

Re: how do you sketh this punch?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Great, and as the user that asked the question, you can mark his answer as the solution.  You should see an "Accept As Solution" button on Tushar's reply... Click it to accept it as the solution.

 

Thanks,



Ken
Production: SE 2019 MP4, Testing: SE 2020
http://Grundey.blogspot.com

Re: how do you sketch this punch?

MLombard
Retired

Yeah, I gotta back Ken up here. It's really helpful when you mark answers as such, because the next time someone has a similar question, we've already got an answer for them. So if someone helps you out, pass it on, and pay it forward a little. Some day you'll be the one answering questions, and you'll want to get a little credit.

Retired Community Manager for Solid Edge. This account is no longer active.

Re: how do you sketch this punch?

Creator
Creator

Right. no problem. I am new here but learn fast :-)

Re: how do you sketh this punch?

Creator
Creator

What do you think guys? How does it look? I think it looks fine.