Cancel
Showing results for 
Search instead for 
Did you mean: 

how to add MATERIAL in material table

Pioneer
Pioneer

Dear sir ,

    I have kindly attachad jpeg file please find the attachment .

 

Thanks & Regards

  ANANDAN.G 

 

2 REPLIES 2

Re: how to add MATERIAL in material table

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,

 

 

this seems to be one existing material with no changes in the values.

Therefore neither the save in lib nor the update lib button are active.

 

What happens, if You change the name or one of the values?

 

 

regards

Wolfgang

 

regards
Wolfgang

Re: how to add MATERIAL in material table

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there,

 

As Wolfgang suggests...you need to make some changes to enable the options to Add or Update the library. This is different again in ST7.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000