Cancel
Showing results for 
Search instead for 
Did you mean: 

how to add cross section file

Creator
Creator

I'm working on a special frame and I need to create my own cross section file for the frame. How should I do that? 

8 REPLIES

Re: how to add cross section file

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

There is a Help topic with instructions on how to create the cross section...

 

https://docs.plm.automation.siemens.com/tdoc/se/110/se_help/#uid:xid1129777:xid1325277:index_frames:...



Ken
Production: SE 2019 MP4, Testing: SE 2020
http://Grundey.blogspot.com

Betreff: how to add cross section file

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

HI @silenteagle

 

 

nothing easier than this.

 

Just create a ordered part file with one single extrusion.

This is important.

Not start with a sketch nor add any additional feature as rounds, chamfers, thinwalls etc.

 

Only one extrusion of Your desired profile.

 

That's it!

 

Save it into Your frame library and use it in structure frame design.

 

So, why only one single extrusion?

 

You also can only create a single sketch, but I prefer to have a 3D preview when using those profiles and therefore I just use the protrusion.

 

There is another function You can use, but You must not use, and this is the "Add Frame Origin Point"

Using this You can define Your preferred origin point rather than the cross section center

regards
Wolfgang

Betreff: how to add cross section file

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

"There is another function You can use, but You must not use,"

@hawcad  I assume by "you must not use", you meant "don't have to use".

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Betreff: how to add cross section file

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @bshand

 

sorry this is one of the stumbles for non native speakers

Of course the intention was "Youo need not to use!"

 

Is this correct and better?

 

 

 

regards
Wolfgang

Betreff: how to add cross section file

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

"You need not use" would be grammatically correct. And I knew it was your unfamiliarity with all the subtleties of English. It's just that "must not" has quite a different meaning than "need not" so it could sow confusion in the minds of some readers.

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Betreff: how to add cross section file

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @bshand

 

 

no no, I say thanks a lot for correcting me by my wrong usage of words.

 

I'm aware about must and must not and the meaning of them or may and may not.

 

The problem was, that sometimes the brain stays German where the hand is trying to write English.

 

I apologize for my mistake and thank for Your help and correction

I think that it is good as well that I'm not aware of all my other errors in my posts but thanksfully would appreciate any assistance

regards
Wolfgang

Betreff: how to add cross section file

Phenom
Phenom

Grammars, you guys are discussing thems? Are these they?

Solid Edge 2019
Windows 7 Professional
Nvidia K2200 & Intel Xeon
"You're doing it wrong"

Betreff: how to add cross section file

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Uh oh. We have our work cut out with this one.

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200